TeachmodeProfileMoveBuilderStartStopPositionMethods Enumeration¶
NXOpen.CAM.TeachmodeProfileMoveBuilder.StartStopPositionMethods is an alias for NXOpen.CAM.TeachmodeProfileMoveBuilderStartStopPositionMethods
-
class
NXOpen.CAM.
TeachmodeProfileMoveBuilderStartStopPositionMethods
¶ Bases:
object
the start and stop positioning methods
Enum Members
Enum Member Enum Member Description Drive Use drive geometry start or stop point Point Use selected point Check Use selected check geometry ContourPosition Use end point of last contouring -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-