SurfaceContourBuilderDriveMethodTypes Enumeration¶
NXOpen.CAM.SurfaceContourBuilder.DriveMethodTypes is an alias for NXOpen.CAM.SurfaceContourBuilderDriveMethodTypes
-
class
NXOpen.CAM.
SurfaceContourBuilderDriveMethodTypes
¶ Bases:
object
Available types for Drive Method
Enum Members
Enum Member Enum Member Description Undef Undefined Curve Curve/Point Spiral Spiral Boundary Boundary AreaMilling Area Milling SurfaceArea Surface Area InterpolatedToolPath Interpolated tool path ToolPath Tool Path RadialCut Radial Cut ContourProfile Contour Profile FlowCut Flow Cut Text Text UserDefined User Function BladeRough Blade Rough BladeFinish Blade Finish HubFinish Hub Finish BlendFinish Blend Finish EdgeFinish Edge Finish RotaryFloorFinish Rotary Floor Finish TubeFinish Tube Finish FreeForm Free Form FreeFormBuildup Free Form Buildup GuidedCurve Guided Curve TubeRough Tube Rough TubeAdditiveThinwall Tube Additive Thinwall TubeAdditive Tube Additive -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-