SurfaceContourBuilderCleanupTypes Enumeration

NXOpen.CAM.SurfaceContourBuilder.CleanupTypes is an alias for NXOpen.CAM.SurfaceContourBuilderCleanupTypes

class NXOpen.CAM.SurfaceContourBuilderCleanupTypes

Bases: object

Available types for cleanup

Enum Members

Enum Member Enum Member Description
Off
UncutValley
SteepArea
Both
FlowcutContacts
FlowcutToolend
FlowcutBoth
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.