SurfaceContourBuilderAccessVectorMethodType Enumeration¶
NXOpen.CAM.SurfaceContourBuilder.AccessVectorMethodType is an alias for NXOpen.CAM.SurfaceContourBuilderAccessVectorMethodType
-
class
NXOpen.CAM.
SurfaceContourBuilderAccessVectorMethodType
¶ Bases:
object
Available types for access vector for the contour profile method of surface milling
Enum Members
Enum Member Enum Member Description Zm positive z-direction of MCS NegZm negative z-direction of MCS Specify user specified AwayFromLine away from the vector defined TowardLine toward the vector defined -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-