StepoverBuilderStepoverTypes Enumeration¶
NXOpen.CAM.StepoverBuilder.StepoverTypes is an alias for NXOpen.CAM.StepoverBuilderStepoverTypes
-
class
NXOpen.CAM.
StepoverBuilderStepoverTypes
¶ Bases:
object
stepover options
New in version NX6.0.0.
Enum Members
Enum Member Enum Member Description NotSet None Constant Constant Scallop Scallop PercentToolFlat % Tool Flat Multiple Multiple Number Number of stepovers Maximum Maximum Stepover Angular Angular VariableAverage Variable Average VariableMaximum Variable Maximum UseCutDepth Use Depth Of Cut PercentRemaining Percent Of Remaining PercentWire % Wire StockPerPass Stock Per Pass PercentThreadLength Percent Thread Length Exact Exact PercentFluteLength Percent Flute Length BlankContourConstant Depth and Number of levels Degression Degression PercentDegression % Degression UserDefined User Defined -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-