SpringPasses Class¶
-
class
NXOpen.CAM.
SpringPasses
¶ Bases:
NXOpen.TaggedObject
Represents a spring passes
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Number | Returns or sets the number of spring passes |
Tag | Returns the Tag for this object. |
Type | Returns or sets the type of spring passes |
Methods¶
Enumerations¶
SpringPassesTypes Enumeration | the alternate spring passes options |
Property Detail¶
Number¶
-
SpringPasses.
Number
¶ Returns or sets the number of spring passes
-------------------------------------
Getter Method
Signature
Number
Returns: the number of spring passes Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Number
Parameters: springPasses (int) – the number of spring passes New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
Type¶
-
SpringPasses.
Type
¶ Returns or sets the type of spring passes
-------------------------------------
Getter Method
Signature
Type
Returns: the type of spring passes Return type: NXOpen.CAM.SpringPassesTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type
Parameters: alternateSpringPassesMode ( NXOpen.CAM.SpringPassesTypes
) – the type of spring passesNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)