SplitSubopCommandLinePlaneTypes Enumeration¶
NXOpen.CAM.SplitSubopCommand.LinePlaneTypes is an alias for NXOpen.CAM.SplitSubopCommandLinePlaneTypes
-
class
NXOpen.CAM.
SplitSubopCommandLinePlaneTypes
¶ Bases:
object
Available line plane types
Enum Members
Enum Member Enum Member Description ParallelToToolaxis Line plane parallel to tool axis NormalToToolaxis Line plane normal to tool axis SpecifyAngle Line plane specify angle -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-