SimulationOptionsBuilderToolShapeMR Enumeration¶
NXOpen.CAM.SimulationOptionsBuilder.ToolShapeMR is an alias for NXOpen.CAM.SimulationOptionsBuilderToolShapeMR
-
class
NXOpen.CAM.
SimulationOptionsBuilderToolShapeMR
¶ Bases:
object
The tool shape for material removal options
Enum Members
Enum Member Enum Member Description Parameter use parametric tool shape Assembly use assembly tool shape -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-