SequenceTypes Enumeration

NXOpen.CAM.Sequence.Types is an alias for NXOpen.CAM.SequenceTypes

class NXOpen.CAM.SequenceTypes

Bases: object

Available types for Sequencing

New in version NX7.5.0.

Enum Members

Enum Member Enum Member Description
InsideOut Inside-Out
OutsideIn Outside-In
SteepLast STEEP Last
SteepFirst STEEP First
InsideOutAlternate Inside-Out Alternate
OutsideInAlternate Outside-In Alternate
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.