RoughTurningBuilderReversalModeTypes Enumeration¶
NXOpen.CAM.RoughTurningBuilder.ReversalModeTypes is an alias for NXOpen.CAM.RoughTurningBuilderReversalModeTypes
-
class
NXOpen.CAM.
RoughTurningBuilderReversalModeTypes
¶ Bases:
object
the Reversal Mode types
New in version NX6.0.0.
Enum Members
Enum Member Enum Member Description AsLevel Reversal mode: As Level Inverse Reversal mode: Inverse Closest Reversal mode: Closest CutLater Reversal mode: Cut Later Omit Reversal mode: Omit -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-