RoughFinishTurningBuilderExtendModeTypes Enumeration¶
NXOpen.CAM.RoughFinishTurningBuilder.ExtendModeTypes is an alias for NXOpen.CAM.RoughFinishTurningBuilderExtendModeTypes
-
class
NXOpen.CAM.
RoughFinishTurningBuilderExtendModeTypes
¶ Bases:
object
the Extend Mode types
New in version NX6.0.0.
Enum Members
Enum Member Enum Member Description Specify Specify Tagential Tagential Tangential Tangential -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-