RoughFinishTurningBuilderCutRegionsTypes Enumeration¶
NXOpen.CAM.RoughFinishTurningBuilder.CutRegionsTypes is an alias for NXOpen.CAM.RoughFinishTurningBuilderCutRegionsTypes
-
class
NXOpen.CAM.
RoughFinishTurningBuilderCutRegionsTypes
¶ Bases:
object
the Cut regions types
New in version NX6.0.0.
Enum Members
Enum Member Enum Member Description SingleRegion Cut regions type: Single Region SingleDirection Cut regions type: Single Direction ReverseDirection Cut regions type: Reverse Direction BiDirectional Cut regions type: Bi-directional Alternate Cut regions type: Alternate -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-