RotaryFinishGeomBuilderPartAxisOfRotationTypes Enumeration¶
NXOpen.CAM.RotaryFinishGeomBuilder.PartAxisOfRotationTypes is an alias for NXOpen.CAM.RotaryFinishGeomBuilderPartAxisOfRotationTypes
-
class
NXOpen.CAM.
RotaryFinishGeomBuilderPartAxisOfRotationTypes
¶ Bases:
object
Available types for Part Axis of Rotation
Enum Members
Enum Member Enum Member Description Zm +ZM Specify Specify Xm +XM Ym +YM -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-