ReliefPlunge Class¶
-
class
NXOpen.CAM.
ReliefPlunge
¶ Bases:
NXOpen.TaggedObject
Represents a
NXOpen.CAM.ReliefPlunge
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Distance | Returns or sets the relief plunge distance |
Tag | Returns the Tag for this object. |
Type | Returns or sets the relief plunge type |
Unit | Returns or sets the relief plunge unit |
Methods¶
Enumerations¶
ReliefPlungeTypes Enumeration | the relief plunge options |
ReliefPlungeUnitTypes Enumeration | the relief plunge options |
Property Detail¶
Distance¶
-
ReliefPlunge.
Distance
¶ Returns or sets the relief plunge distance
-------------------------------------
Getter Method
Signature
Distance
Returns: the relief plunge distance Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Distance
Parameters: distance (float) – the relief plunge distance New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
Type¶
-
ReliefPlunge.
Type
¶ Returns or sets the relief plunge type
-------------------------------------
Getter Method
Signature
Type
Returns: the relief plunge mode Return type: NXOpen.CAM.ReliefPlungeTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type
Parameters: reliefPlungeValue ( NXOpen.CAM.ReliefPlungeTypes
) – the relief plunge modeNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
Unit¶
-
ReliefPlunge.
Unit
¶ Returns or sets the relief plunge unit
-------------------------------------
Getter Method
Signature
Unit
Returns: the relief plunge unit Return type: NXOpen.CAM.ReliefPlungeUnitTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Unit
Parameters: reliefPlungeUnit ( NXOpen.CAM.ReliefPlungeUnitTypes
) – the relief plunge unitNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)