ProjVecCiBuilderDpmProjTypes Enumeration¶
NXOpen.CAM.ProjVecCiBuilder.DpmProjTypes is an alias for NXOpen.CAM.ProjVecCiBuilderDpmProjTypes
-
class
NXOpen.CAM.
ProjVecCiBuilderDpmProjTypes
¶ Bases:
object
Available types for Project Vector
Enum Members
Enum Member Enum Member Description ProjVecFixed Specify Vector ProjVecToolAxis Tool Axis ProjVecFromPoint way from Point ProjVecToPoint Toward Point ProjVecFromLine Away from Line ProjVecToLine Toward Line ProjVecNormToDrive Normal to Drive ProjVecToDrive Toward Drive ProjVecRuling Swarf Ruling ProjVecUserDefined User Function ProjVecToolAxisUp Tool Axis up ProjVecTotal Total -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-