ProbeInspectPointMoveBuilderDirection Enumeration¶
NXOpen.CAM.ProbeInspectPointMoveBuilder.Direction is an alias for NXOpen.CAM.ProbeInspectPointMoveBuilderDirection
-
class
NXOpen.CAM.
ProbeInspectPointMoveBuilderDirection
¶ Bases:
object
the probing direction type
Enum Members
Enum Member Enum Member Description Inferred Inferred using surface normal Xm XM Negxm Negative XM Ym YM Negym Negative YM Zm ZM Negzm Negative ZM -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-