PmopToolAxisCiBuilder Class¶
-
class
NXOpen.CAM.
PmopToolAxisCiBuilder
¶ Bases:
NXOpen.TaggedObject
Represents a PmopToolAxisCiBuilder
This is an abstract class, and cannot be instantiated.
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
FixedVector | Returns or sets the tool axis vector |
Tag | Returns the Tag for this object. |
ToolAxis | Returns or sets the tool axis type |
Methods¶
Enumerations¶
PmopToolAxisCiBuilderToolAxisTypes Enumeration | Available types for pmop tool axis type |
Property Detail¶
FixedVector¶
-
PmopToolAxisCiBuilder.
FixedVector
¶ Returns or sets the tool axis vector
-------------------------------------
Getter Method
Signature
FixedVector
Returns: Return type: NXOpen.SmartObject
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FixedVector
Parameters: newValue ( NXOpen.SmartObject
) –New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
ToolAxis¶
-
PmopToolAxisCiBuilder.
ToolAxis
¶ Returns or sets the tool axis type
-------------------------------------
Getter Method
Signature
ToolAxis
Returns: the tool axis type Return type: NXOpen.CAM.PmopToolAxisCiBuilderToolAxisTypes
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToolAxis
Parameters: newValue ( NXOpen.CAM.PmopToolAxisCiBuilderToolAxisTypes
) – the tool axis typeNew in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)