PatternTypeBuilderOption Enumeration¶
NXOpen.CAM.PatternTypeBuilder.Option is an alias for NXOpen.CAM.PatternTypeBuilderOption
-
class
NXOpen.CAM.
PatternTypeBuilderOption
¶ Bases:
object
Enum of pattern type
Enum Members
Enum Member Enum Member Description NotSet Pattern is not classified Offset Pattern is created by offsetting from one curve Morph Pattern is created by morphing between curves OffsetAroundShortGuide Pattern is created by offsetting around one curve -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-