PathLevelMarker Class¶
-
class
NXOpen.CAM.
PathLevelMarker
¶ Bases:
NXOpen.TransientObject
This class represents the data of a Linear Motion
New in version NX10.0.3.
Properties¶
Property | Description |
---|---|
LevelDepth | Returns or sets the level depth |
LevelNormal | Returns or sets the level normal |
LevelNumber | Returns or sets the level number |
OperationName | Returns or sets the operation name |
Property Detail¶
LevelDepth¶
-
PathLevelMarker.
LevelDepth
¶ Returns or sets the level depth
-------------------------------------
Getter Method
Signature
LevelDepth
Returns: Return type: float New in version NX10.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
LevelDepth
Parameters: levelDepth (float) – New in version NX10.0.3.
License requirements: None.
LevelNormal¶
-
PathLevelMarker.
LevelNormal
¶ Returns or sets the level normal
-------------------------------------
Getter Method
Signature
LevelNormal
Returns: Return type: NXOpen.Vector3d
New in version NX10.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
LevelNormal
Parameters: levelNormal ( NXOpen.Vector3d
) –New in version NX10.0.3.
License requirements: None.
LevelNumber¶
-
PathLevelMarker.
LevelNumber
¶ Returns or sets the level number
-------------------------------------
Getter Method
Signature
LevelNumber
Returns: Return type: int New in version NX11.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
LevelNumber
Parameters: levelnumber (int) – New in version NX11.0.2.
License requirements: None.
OperationName¶
-
PathLevelMarker.
OperationName
¶ Returns or sets the operation name
-------------------------------------
Getter Method
Signature
OperationName
Returns: Return type: str New in version NX11.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
OperationName
Parameters: operName (str) – New in version NX11.0.2.
License requirements: None.
Method Detail¶
Dispose¶
-
PathLevelMarker.
Dispose
¶ Free resources associated with the instance.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX10.0.3.
License requirements: None.