PathLaserGeometryData Class¶
-
class
NXOpen.CAM.
PathLaserGeometryData
¶ Bases:
NXOpen.TransientObject
Definition for Laser geometry data
New in version NX9.0.3.
Methods¶
Method | Description |
---|---|
Dispose | Free resources associated with the instance. |
GetAmFeatureBody | Get the am feature body |
GetInProcessBodies | Get the in process bodies |
GetNumberOfInProcessBodies | Get the number of in process bodies |
Method Detail¶
Dispose¶
-
PathLaserGeometryData.
Dispose
¶ Free resources associated with the instance.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX9.0.3.
License requirements: None.
GetAmFeatureBody¶
-
PathLaserGeometryData.
GetAmFeatureBody
¶ Get the am feature body
Signature
GetAmFeatureBody()
Returns: Return type: NXOpen.TaggedObject
New in version NX9.0.3.
License requirements: None.
GetInProcessBodies¶
-
PathLaserGeometryData.
GetInProcessBodies
¶ Get the in process bodies
Signature
GetInProcessBodies()
Returns: Return type: list of NXOpen.TaggedObject
New in version NX9.0.3.
License requirements: None.