PathLaserDepositionData Class¶
-
class
NXOpen.CAM.
PathLaserDepositionData
¶ Bases:
NXOpen.TransientObject
Definition for Laser deposition data
New in version NX9.0.3.
Methods¶
Method | Description |
---|---|
Dispose | Free resources associated with the instance. |
GetLaserWidth | Get the laser width |
GetLayerThickness | Get the layer thickness |
Method Detail¶
Dispose¶
-
PathLaserDepositionData.
Dispose
¶ Free resources associated with the instance.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX9.0.3.
License requirements: None.