PathEvent Class¶
-
class
NXOpen.CAM.
PathEvent
¶ Bases:
NXOpen.TransientObject
Represets a Cam Tool Path Event
This is a Subobject and cannot be publicly instantiated.
New in version NX11.0.2.
Methods¶
Method | Description |
---|---|
Dispose | Free resources associated with the instance. |
GetNext | Get the next tool path event, will return None to indicate end of list. |
GetPrevious | Get the previous tool path event, will return None to indicate start of list. |
Method Detail¶
Dispose¶
-
PathEvent.
Dispose
¶ Free resources associated with the instance.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX11.0.2.
License requirements: None.
GetNext¶
-
PathEvent.
GetNext
¶ Get the next tool path event, will return None to indicate end of list.
Signature
GetNext()
Returns: Return type: NXOpen.CAM.PathEvent
New in version NX11.0.2.
License requirements: None.
GetPrevious¶
-
PathEvent.
GetPrevious
¶ Get the previous tool path event, will return None to indicate start of list.
Signature
GetPrevious()
Returns: Return type: NXOpen.CAM.PathEvent
New in version NX11.0.2.
License requirements: None.