PathContactMotion Class¶
-
class
NXOpen.CAM.
PathContactMotion
¶ Bases:
NXOpen.TransientObject
This class represents the data of a Linear Motion
New in version NX11.0.2.
Properties¶
Property | Description |
---|---|
ArcAxis | Returns or sets the axis of the arc of the contact motion if the shape is circular |
ArcCenter | Returns or sets the center of the arc of the contact motion if the shape is circular |
ArcDirection | Returns or sets the direction of the arc of the contact motion if the shape is circular |
ArcRadius | Returns or sets the radius of the arc of the contact motion if the shape is circular |
MotionShape | Returns or sets the motion shape |
Point | Returns or sets the point of the contact motion |
Property Detail¶
ArcAxis¶
-
PathContactMotion.
ArcAxis
¶ Returns or sets the axis of the arc of the contact motion if the shape is circular
-------------------------------------
Getter Method
Signature
ArcAxis
Returns: Return type: NXOpen.Vector3d
New in version NX11.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
ArcAxis
Parameters: arcAxis ( NXOpen.Vector3d
) –New in version NX11.0.2.
License requirements: cam_base (“CAM BASE”)
ArcCenter¶
-
PathContactMotion.
ArcCenter
¶ Returns or sets the center of the arc of the contact motion if the shape is circular
-------------------------------------
Getter Method
Signature
ArcCenter
Returns: Return type: NXOpen.Point3d
New in version NX11.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
ArcCenter
Parameters: arcCenter ( NXOpen.Point3d
) –New in version NX11.0.2.
License requirements: cam_base (“CAM BASE”)
ArcDirection¶
-
PathContactMotion.
ArcDirection
¶ Returns or sets the direction of the arc of the contact motion if the shape is circular
-------------------------------------
Getter Method
Signature
ArcDirection
Returns: Return type: NXOpen.CAM.CamPathDir
New in version NX11.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
ArcDirection
Parameters: arcDirection ( NXOpen.CAM.CamPathDir
) –New in version NX11.0.2.
License requirements: cam_base (“CAM BASE”)
ArcRadius¶
-
PathContactMotion.
ArcRadius
¶ Returns or sets the radius of the arc of the contact motion if the shape is circular
-------------------------------------
Getter Method
Signature
ArcRadius
Returns: Return type: float New in version NX11.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
ArcRadius
Parameters: arcRadius (float) – New in version NX11.0.2.
License requirements: cam_base (“CAM BASE”)
MotionShape¶
-
PathContactMotion.
MotionShape
¶ Returns or sets the motion shape
-------------------------------------
Getter Method
Signature
MotionShape
Returns: Return type: NXOpen.CAM.CamPathContactMotionShapeType
New in version NX11.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
MotionShape
Parameters: motionShape ( NXOpen.CAM.CamPathContactMotionShapeType
) –New in version NX11.0.2.
License requirements: cam_base (“CAM BASE”)
Point¶
-
PathContactMotion.
Point
¶ Returns or sets the point of the contact motion
-------------------------------------
Getter Method
Signature
Point
Returns: Return type: NXOpen.Point3d
New in version NX11.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
Point
Parameters: endPoint ( NXOpen.Point3d
) –New in version NX11.0.2.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
Dispose¶
-
PathContactMotion.
Dispose
¶ Free resources associated with the instance.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX11.0.2.
License requirements: None.