PathCircularMotion Class¶
-
class
NXOpen.CAM.
PathCircularMotion
¶ Bases:
NXOpen.CAM.PathLinearMotion
This class represents the data of a Linear Motion
New in version NX10.0.1.
Properties¶
Property | Description |
---|---|
ArcAxis | Returns or sets the axis of the arc motion |
ArcCenter | Returns or sets the center of the arc motion |
ArcRadius | Returns or sets the radius of the arc motion |
ContactData | Returns or sets the contact motion if the motion is contact and Nothing if not |
Direction | Returns or sets the direction of the arc motion |
EndPoint | Returns or sets the end point of the motion |
IsContact | Returns or sets the check to see if motion is contact |
IsCustomFeedrate | Returns or sets the custom feed rate indicator |
MotionType | Returns or sets the motion type |
ToolAxis | Returns or sets the tool axis of the motion |
Methods¶
Method | Description |
---|---|
Dispose | Free resources associated with the instance. |
GetFeedrate | Get feed rate information |
SetFeedrate | Set feed rate information. |
Property Detail¶
ArcAxis¶
-
PathCircularMotion.
ArcAxis
¶ Returns or sets the axis of the arc motion
-------------------------------------
Getter Method
Signature
ArcAxis
Returns: Return type: NXOpen.Vector3d
New in version NX10.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ArcAxis
Parameters: arcAxis ( NXOpen.Vector3d
) –New in version NX10.0.1.
License requirements: cam_base (“CAM BASE”)
ArcCenter¶
-
PathCircularMotion.
ArcCenter
¶ Returns or sets the center of the arc motion
-------------------------------------
Getter Method
Signature
ArcCenter
Returns: Return type: NXOpen.Point3d
New in version NX10.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ArcCenter
Parameters: arcCenter ( NXOpen.Point3d
) –New in version NX10.0.1.
License requirements: cam_base (“CAM BASE”)
ArcRadius¶
-
PathCircularMotion.
ArcRadius
¶ Returns or sets the radius of the arc motion
-------------------------------------
Getter Method
Signature
ArcRadius
Returns: Return type: float New in version NX10.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ArcRadius
Parameters: arcRadius (float) – New in version NX10.0.1.
License requirements: cam_base (“CAM BASE”)
Direction¶
-
PathCircularMotion.
Direction
¶ Returns or sets the direction of the arc motion
-------------------------------------
Getter Method
Signature
Direction
Returns: Return type: NXOpen.CAM.CamPathDir
New in version NX10.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
Direction
Parameters: arcDirection ( NXOpen.CAM.CamPathDir
) –New in version NX10.0.1.
License requirements: cam_base (“CAM BASE”)