OperationTeaching Class¶
-
class
NXOpen.CAM.
OperationTeaching
¶ Bases:
NXOpen.Builder
Represents a OperationTeaching Builder
To create a new instance of this class, use
NXOpen.CAM.CAMSetup.CreateOperationTeaching()
New in version NX8.0.0.
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Gets the selected feature |
GetLibraryPath | Gets the selected library path |
GetObject | Returns the object currently being edited by this builder. |
GetOperations | Gets the selected operations |
SetFeature | Sets the selected feature |
SetLibraryPath | Sets the selected library path |
SetOperations | Sets the selected operations |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Teach | Teaches the new operations |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
GetFeature¶
-
OperationTeaching.
GetFeature
¶ Gets the selected feature
Signature
GetFeature()
Returns: Return type: NXOpen.CAM.CAMFeature
New in version NX8.0.0.
License requirements: fbm_author (“FBM Author”)
GetLibraryPath¶
-
OperationTeaching.
GetLibraryPath
¶ Gets the selected library path
Signature
GetLibraryPath()
Returns: Return type: str New in version NX8.0.0.
License requirements: fbm_author (“FBM Author”)
GetOperations¶
-
OperationTeaching.
GetOperations
¶ Gets the selected operations
Signature
GetOperations()
Returns: Return type: list of NXOpen.CAM.Operation
New in version NX8.0.0.
License requirements: fbm_author (“FBM Author”)
SetFeature¶
-
OperationTeaching.
SetFeature
¶ Sets the selected feature
Signature
SetFeature(feature)
Parameters: feature ( NXOpen.CAM.CAMFeature
) –New in version NX8.0.0.
License requirements: fbm_author (“FBM Author”)
SetLibraryPath¶
-
OperationTeaching.
SetLibraryPath
¶ Sets the selected library path
Signature
SetLibraryPath(path)
Parameters: path (str) – New in version NX8.0.0.
License requirements: fbm_author (“FBM Author”)
SetOperations¶
-
OperationTeaching.
SetOperations
¶ Sets the selected operations
Signature
SetOperations(aOperations)
Parameters: aOperations (list of NXOpen.CAM.Operation
) –New in version NX8.0.0.
License requirements: fbm_author (“FBM Author”)
Teach¶
-
OperationTeaching.
Teach
¶ Teaches the new operations
Signature
Teach()
Returns: Return type: list of str New in version NX8.0.0.
License requirements: fbm_author (“FBM Author”)
Validate¶
-
OperationTeaching.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.