NcmWedmBuilderLeadInMethodTypes Enumeration¶
NXOpen.CAM.NcmWedmBuilder.LeadInMethodTypes is an alias for NXOpen.CAM.NcmWedmBuilderLeadInMethodTypes
-
class
NXOpen.CAM.
NcmWedmBuilderLeadInMethodTypes
¶ Bases:
object
the types available for lead in method
New in version NX7.5.0.
Enum Members
Enum Member Enum Member Description Direct direct lead in Angular angular lead in Circular circular lead in -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-