NcmTurnThreadBuilderLocalReturnTypes Enumeration¶
NXOpen.CAM.NcmTurnThreadBuilder.LocalReturnTypes is an alias for NXOpen.CAM.NcmTurnThreadBuilderLocalReturnTypes
-
class
NXOpen.CAM.
NcmTurnThreadBuilderLocalReturnTypes
¶ Bases:
object
The Cut regions type options
New in version NX6.0.0.
Enum Members
Enum Member Enum Member Description NotSet None Direct Direct RadialAxial Radial-Axial AxialRadial Axial-Radial ClearRadialDirect Clear Radial-Direct ClearAxialDirect Clear Axial-Direct ClearRadial Clear Radial ClearAxial Clear Axial RadialClearAxialDirect Radial-Clear Axial-Direct RadialAxialRadial Radial-Axial-Radial RadialClearAxial Radial-Clear Axial ClearRadialClearAxialDirect Clear Radial-Clear Axial-Direct ClearRadialAxialRadial Clear Radial-Axial-Radial ClearRadialClearAxial Clear Radial-Clear Axial -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-