NcmTransferBuilderTraverseTypes Enumeration¶
NXOpen.CAM.NcmTransferBuilder.TraverseTypes is an alias for NXOpen.CAM.NcmTransferBuilderTraverseTypes
-
class
NXOpen.CAM.
NcmTransferBuilderTraverseTypes
¶ Bases:
object
Available types for traverse
Enum Members
Enum Member Enum Member Description Same traverse setting from between regions ShortestToClearance traverse shortest to clearance LowestSafeZ traverse at lowest safe z Direct traverse direct Smooth traverse smooth spline -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-