NcmTransferBuilderAppDepMethodTypes Enumeration¶
NXOpen.CAM.NcmTransferBuilder.AppDepMethodTypes is an alias for NXOpen.CAM.NcmTransferBuilderAppDepMethodTypes
-
class
NXOpen.CAM.
NcmTransferBuilderAppDepMethodTypes
¶ Bases:
object
Available methods for approach and departure
Enum Members
Enum Member Enum Member Description Same use setting from transfer between regions NotSet none AlongToolAxis along tool axis AlongVector along vector ToolAxisClearance along tool axis from/to clearance ShortestDistanceClearance shortest distance from/to clearance VectorClearance along vector from/to clearance TangentClearance tangent from/to clearance Automatic automatic -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-