NcmScEngRetBuilderEngRetTypes Enumeration¶
NXOpen.CAM.NcmScEngRetBuilder.EngRetTypes is an alias for NXOpen.CAM.NcmScEngRetBuilderEngRetTypes
-
class
NXOpen.CAM.
NcmScEngRetBuilderEngRetTypes
¶ Bases:
object
Available types for engage/retract in surface contouring
Enum Members
Enum Member Enum Member Description SameAsDefault Same as Default SameAsEngage Same as Engage (only for retract) Linear Linear LinearAlongVector Linear - Along Vector LinearNormalToPart Linear - Normal to Part ArcParallelToToolAxis Arc - Parallel to Tool Axis ArcNormalToToolAxis Arc - Normal to Tool Axis ArcTangentToApproach Arc - Tangent to Approach ArcNormalToPart Arc - Normal to Part HelicalClw Helical Clockwise HelicalCclw Helical Counter Clockwise PlungeLift Plunge Engage/Lift Retract NotSet None Points to-from point Smooth Smooth connections -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-