NcmPlanarEngRetBuilderMinClearanceTypes Enumeration¶
NXOpen.CAM.NcmPlanarEngRetBuilder.MinClearanceTypes is an alias for NXOpen.CAM.NcmPlanarEngRetBuilderMinClearanceTypes
-
class
NXOpen.CAM.
NcmPlanarEngRetBuilderMinClearanceTypes
¶ Bases:
object
Available types for the Minimum Clearance
Enum Members
Enum Member Enum Member Description NotSet None ExtendAndTrim Extend and trim ExtendOnly Extend only SameAsOpenEngage Same as open engage SameAsRetract Same as retract -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-