NcmPlanarEngRetBuilderEngRetTypes Enumeration¶
NXOpen.CAM.NcmPlanarEngRetBuilder.EngRetTypes is an alias for NXOpen.CAM.NcmPlanarEngRetBuilderEngRetTypes
-
class
NXOpen.CAM.
NcmPlanarEngRetBuilderEngRetTypes
¶ Bases:
object
Available types for engage/retract in Planar Milling
Enum Members
Enum Member Enum Member Description SameAsDefault Same as Default (Inherit) SameAsClosed Same as Closed Engage (from open) SameAsEngage Same as (Open) Engage (from retract) Helical Helical Ramp RampOnShape Ramp on shape ZigzagRamp ZigZag Ramp Linear Linear Arc Arc ArcParallelToToolAxis Arc - Parallel to Tool Axis ArcNormalToToolAxis Arc - Normal to Tool Axis ArcNormalToPart Arc - Normal to Part HighSpeedArc High Speed Arcs Points to-from points PlungeLift Plunge Engage/Lift Retract AlongVector Vector Dist AngAngPlane Linear to plane VectorPlane Vector to plane NotSet None LinearRelativeCut Linear relative to cut direction Smooth Smooth -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-