NcmHoleMachiningInitialTypes Enumeration¶
NXOpen.CAM.NcmHoleMachining.InitialTypes is an alias for NXOpen.CAM.NcmHoleMachiningInitialTypes
-
class
NXOpen.CAM.
NcmHoleMachiningInitialTypes
¶ Bases:
object
Available types for initial clearance in hole machining
Enum Members
Enum Member Enum Member Description Clearance Clearance - Tool Axis Distance distance NotSet none BlankPlane blank plane ClearanceShortestDistance Clearance - Shortest Distance ClearanceCutPlane Clearance - Cut Plane -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-