NcmEngRetBuilderEngageRetractTypes Enumeration¶
NXOpen.CAM.NcmEngRetBuilder.EngageRetractTypes is an alias for NXOpen.CAM.NcmEngRetBuilderEngageRetractTypes
-
class
NXOpen.CAM.
NcmEngRetBuilderEngageRetractTypes
¶ Bases:
object
Available types for engage/retract in surface contouring
Enum Members
Enum Member Enum Member Description Linear Linear PlungeLift Plunge Engage/Lift Retract Smooth Smooth connections NotSet None -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-