NCGroupCollectionUseDefaultName Enumeration¶
NXOpen.CAM.NCGroupCollection.UseDefaultName is an alias for NXOpen.CAM.NCGroupCollectionUseDefaultName
-
class
NXOpen.CAM.
NCGroupCollectionUseDefaultName
¶ Bases:
object
Whether use the default name in creation
Enum Members
Enum Member Enum Member Description False don’t user the default name True use the default name -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-