MultiplePassesBuilderStepMethodTypes Enumeration

NXOpen.CAM.MultiplePassesBuilder.StepMethodTypes is an alias for NXOpen.CAM.MultiplePassesBuilderStepMethodTypes

class NXOpen.CAM.MultiplePassesBuilderStepMethodTypes

Bases: object

Available types for Step Method

Enum Members

Enum Member Enum Member Description
Increment Increment
Passes Passes
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.