MultiplePassesBuilderOrderTypes Enumeration

NXOpen.CAM.MultiplePassesBuilder.OrderTypes is an alias for NXOpen.CAM.MultiplePassesBuilderOrderTypes

class NXOpen.CAM.MultiplePassesBuilderOrderTypes

Bases: object

Available types for Order

Enum Members

Enum Member Enum Member Description
SidePassesFirst Side First
DepthPassesFirst Depth First
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.