MultiRampTypes Enumeration

NXOpen.CAM.MultiRamp.Types is an alias for NXOpen.CAM.MultiRampTypes

class NXOpen.CAM.MultiRampTypes

Bases: object

the multi ramp pattern types

New in version NX6.0.0.

Enum Members

ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.