MinCutLength Class¶
-
class
NXOpen.CAM.
MinCutLength
¶ Bases:
NXOpen.TaggedObject
Represents a
NXOpen.CAM.MinCutLength
Properties¶
Property | Description |
---|---|
Distance | Returns or sets the distance of Minimum Cut Length |
Status | Returns or sets the status of Minimum Cut Length |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
MinCutLengthTypes Enumeration | the mininmum cut length options |
Property Detail¶
Distance¶
-
MinCutLength.
Distance
¶ Returns or sets the distance of Minimum Cut Length
-------------------------------------
Getter Method
Signature
Distance
Returns: the distance of Minimum Cut Length Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Distance
Parameters: minLength (float) – the distance of Minimum Cut Length New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
Status¶
-
MinCutLength.
Status
¶ Returns or sets the status of Minimum Cut Length
-------------------------------------
Getter Method
Signature
Status
Returns: the status of Minimum Cut Length Return type: NXOpen.CAM.MinCutLengthTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Status
Parameters: minLength ( NXOpen.CAM.MinCutLengthTypes
) – the the status of Minimum Cut LengthNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)