MillingToolBuilderToolDirectionTypes Enumeration¶
NXOpen.CAM.MillingToolBuilder.ToolDirectionTypes is an alias for NXOpen.CAM.MillingToolBuilderToolDirectionTypes
-
class
NXOpen.CAM.
MillingToolBuilderToolDirectionTypes
¶ Bases:
object
Available types for tool direction milling tool
Enum Members
Enum Member Enum Member Description NotSet None Clw CLW Cclw CCLW -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-