MillToolBuilderCutterSubtypes Enumeration¶
NXOpen.CAM.MillToolBuilder.CutterSubtypes is an alias for NXOpen.CAM.MillToolBuilderCutterSubtypes
-
class
NXOpen.CAM.
MillToolBuilderCutterSubtypes
¶ Bases:
object
Available types for mill tool subtype
Enum Members
Enum Member Enum Member Description Mill5 5-Parameter Mill7 7-Parameter Mill10 10-Parameter MillBall Ball MillTool ChamferTool Chamfer MillTool SphericalMill Spherical MillTool -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-