MillOperationBuilderWallCleanupTypes Enumeration¶
NXOpen.CAM.MillOperationBuilder.WallCleanupTypes is an alias for NXOpen.CAM.MillOperationBuilderWallCleanupTypes
-
class
NXOpen.CAM.
MillOperationBuilderWallCleanupTypes
¶ Bases:
object
the wall cleanup modes
New in version NX12.0.0.
Enum Members
Enum Member Enum Member Description NotSet wall cleanup: none AtStart wall cleanup: at start AtEnd wall cleanup: at end Automatic wall cleanup: automatic; not valid for surface contour - boundary drive method -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-