LaserPiercingPoint Class¶
-
class
NXOpen.CAM.
LaserPiercingPoint
¶ Bases:
NXOpen.TaggedObject
Represents piercing point settings for laser move
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
Point | Returns or sets the Piercing Point |
PointType | Returns or sets the Piercing Point Type |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
LaserPiercingPointTypes Enumeration | the Piercing Point enum |
Property Detail¶
Point¶
-
LaserPiercingPoint.
Point
¶ Returns or sets the Piercing Point
-------------------------------------
Getter Method
Signature
Point
Returns: the piercing point Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Point
Parameters: newValue ( NXOpen.Point
) – the piercing pointNew in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
PointType¶
-
LaserPiercingPoint.
PointType
¶ Returns or sets the Piercing Point Type
-------------------------------------
Getter Method
Signature
PointType
Returns: the piercing point type Return type: NXOpen.CAM.LaserPiercingPointTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointType
Parameters: type ( NXOpen.CAM.LaserPiercingPointTypes
) – the piercing point typeNew in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)