IpwAnalysisBuilder Class¶
-
class
NXOpen.CAM.
IpwAnalysisBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAM.IpwAnalysisBuilder
This is an abstract class, and cannot be instantiated.
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
ColorControlType | Returns or sets the control color |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CreateIpwContainmentCurvesBuilder | Creates a list item |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
IpwAnalysisBuilderColorControl Enumeration | the color control type options |
Property Detail¶
ColorControlType¶
-
IpwAnalysisBuilder.
ColorControlType
¶ Returns or sets the control color
-------------------------------------
Getter Method
Signature
ColorControlType
Returns: Return type: NXOpen.CAM.IpwAnalysisBuilderColorControl
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ColorControlType
Parameters: type ( NXOpen.CAM.IpwAnalysisBuilderColorControl
) –New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
CreateIpwContainmentCurvesBuilder¶
-
IpwAnalysisBuilder.
CreateIpwContainmentCurvesBuilder
¶ Creates a list item
Signature
CreateIpwContainmentCurvesBuilder(position)
Parameters: position (int) – position Returns: ipw containment curves builder Return type: NXOpen.CAM.IpwContainmentCurvesBuilder
New in version NX6.0.0.
License requirements: None.
Validate¶
-
IpwAnalysisBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.