InspectionSensorBuilder Class¶
-
class
NXOpen.CAM.
InspectionSensorBuilder
¶ Bases:
NXOpen.CAM.OperationBuilder
Represents the builder for a CMM Inspection Sensor.
To create a new instance of this class, use
NXOpen.CAM.InspectionOperationCollection.CreateInspectionSensorBuilder()
New in version NX7.0.0.
Properties¶
Property | Description |
---|---|
AngleA | Returns or sets the sensor tip location tilt angle component |
AngleB | Returns or sets the sensor tip location rotation angle component |
ChannelName | Returns or sets the channel’s name |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
Description | Returns or sets the description |
EndOfPath | Returns the end event builder |
EndUdeSet | Returns the end ude set |
Geometry | Returns the geometry builder |
GougeChecking | Returns or sets the gouge checking flag |
HoleAxisType | Returns or sets the Hole Axis Type |
HoleDepth | Returns the max depth distance builder |
HoleDepthType | Returns or sets the Hole Depth Type |
LayoutAndLayer | Returns the Layer and Layout |
MasterOpLabel | Returns or sets the master sensor label |
MotionOutputBuilder | Returns the motion output builder |
Notes | Returns the notes builder |
OptimizationBasedOn | Returns or sets the optimization based on in operation |
OptimizationDistanceMethod | Returns or sets the optimization distance method in operation |
OptimizationLevel | Returns or sets the optimization level in operation |
OptimizationMethod | Returns or sets the optim method |
PathDisplayOptions | Returns the path display options builder |
PostToolPathExit | Returns or sets the environment variable that points to the post tool path generation library which has the exit |
RetractDistance | Returns the Retract Distance builder (inheritable double) |
RetractDistanceOnToolAxisChange | Returns the Retract Distance on Tool Axis Change builder (inheritable double) |
SafeClearance | Returns the safe clearance builder |
SelectToolFlag | Returns or sets the user selected tool |
SensorOpLabel | Returns or sets the sensor label |
SensorOpName | Returns or sets the inspection sensor operation name |
SensorTipDiameter | Returns or sets the sensor tip diameter |
SensorTipLength | Returns or sets the sensor tip length |
SensorTipLocation | Returns or sets the sensor tip location method |
SensorTipSize | Returns or sets the sensor tip size |
SensorTipType | Returns or sets the sensor tip type |
SensorType | Returns or sets the sensor type |
StartOfPath | Returns the start event builder |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
TipNumber | Returns or sets the probe tip number |
ToolChangeSetting | Returns the tool change builder |
ToolName | Returns or sets the inspection probe tool name |
ToolPathEditor | Returns the Tool Path Editor Builder |
ToolPathSplitParametersBuilder | Returns the tool path split Parameters |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCustomizableItemBuilder | Returns the customizable item builder for the given customizable item name |
GetCustomizableItemNames | Returns the names for all customizable item ids |
GetHoleAxisValues | Get the Hole Axis values |
GetObject | Returns the object currently being edited by this builder. |
GetSensorTipIjk | Get the sensor tip location vector coordinates |
GetSensorTipXyz | Get the sensor tip location cartesian coordinates |
SetHoleAxisValues | Set the Hole Axis values |
SetSensorTipIjk | Set the sensor tip location vector coordinates |
SetSensorTipXyz | Set the sensor tip location cartesian coordinates |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
InspectionSensorBuilderSensorTipLocationTypes Enumeration | the sensor tip location method |
InspectionSensorBuilderSensorTipTypes Enumeration | the sensor tip type |
InspectionSensorBuilderSensorTypes Enumeration | the sensor type |
Property Detail¶
AngleA¶
-
InspectionSensorBuilder.
AngleA
¶ Returns or sets the sensor tip location tilt angle component
-------------------------------------
Getter Method
Signature
AngleA
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngleA
Parameters: angle (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
AngleB¶
-
InspectionSensorBuilder.
AngleB
¶ Returns or sets the sensor tip location rotation angle component
-------------------------------------
Getter Method
Signature
AngleB
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngleB
Parameters: angle (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
MasterOpLabel¶
-
InspectionSensorBuilder.
MasterOpLabel
¶ Returns or sets the master sensor label
-------------------------------------
Getter Method
Signature
MasterOpLabel
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MasterOpLabel
Parameters: label (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SensorOpLabel¶
-
InspectionSensorBuilder.
SensorOpLabel
¶ Returns or sets the sensor label
-------------------------------------
Getter Method
Signature
SensorOpLabel
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SensorOpLabel
Parameters: label (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SensorOpName¶
-
InspectionSensorBuilder.
SensorOpName
¶ Returns or sets the inspection sensor operation name
-------------------------------------
Getter Method
Signature
SensorOpName
Returns: Return type: str New in version NX7.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
SensorOpName
Parameters: sensorOpName (str) – New in version NX7.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SensorTipDiameter¶
-
InspectionSensorBuilder.
SensorTipDiameter
¶ Returns or sets the sensor tip diameter
-------------------------------------
Getter Method
Signature
SensorTipDiameter
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SensorTipDiameter
Parameters: diameter (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SensorTipLength¶
-
InspectionSensorBuilder.
SensorTipLength
¶ Returns or sets the sensor tip length
-------------------------------------
Getter Method
Signature
SensorTipLength
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SensorTipLength
Parameters: length (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SensorTipLocation¶
-
InspectionSensorBuilder.
SensorTipLocation
¶ Returns or sets the sensor tip location method
-------------------------------------
Getter Method
Signature
SensorTipLocation
Returns: Return type: NXOpen.CAM.InspectionSensorBuilderSensorTipLocationTypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SensorTipLocation
Parameters: type ( NXOpen.CAM.InspectionSensorBuilderSensorTipLocationTypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SensorTipSize¶
-
InspectionSensorBuilder.
SensorTipSize
¶ Returns or sets the sensor tip size
-------------------------------------
Getter Method
Signature
SensorTipSize
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SensorTipSize
Parameters: size (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SensorTipType¶
-
InspectionSensorBuilder.
SensorTipType
¶ Returns or sets the sensor tip type
-------------------------------------
Getter Method
Signature
SensorTipType
Returns: Return type: NXOpen.CAM.InspectionSensorBuilderSensorTipTypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SensorTipType
Parameters: type ( NXOpen.CAM.InspectionSensorBuilderSensorTipTypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SensorType¶
-
InspectionSensorBuilder.
SensorType
¶ Returns or sets the sensor type
-------------------------------------
Getter Method
Signature
SensorType
Returns: Return type: NXOpen.CAM.InspectionSensorBuilderSensorTypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SensorType
Parameters: type ( NXOpen.CAM.InspectionSensorBuilderSensorTypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
TipNumber¶
-
InspectionSensorBuilder.
TipNumber
¶ Returns or sets the probe tip number
-------------------------------------
Getter Method
Signature
TipNumber
Returns: Return type: int New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TipNumber
Parameters: tipNumber (int) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ToolName¶
-
InspectionSensorBuilder.
ToolName
¶ Returns or sets the inspection probe tool name
-------------------------------------
Getter Method
Signature
ToolName
Returns: Return type: str New in version NX7.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToolName
Parameters: toolName (str) – New in version NX7.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Method Detail¶
GetSensorTipIjk¶
-
InspectionSensorBuilder.
GetSensorTipIjk
¶ Get the sensor tip location vector coordinates
Signature
GetSensorTipIjk()
Returns: the ijk values Return type: list of float New in version NX7.0.0.
License requirements: None.
GetSensorTipXyz¶
-
InspectionSensorBuilder.
GetSensorTipXyz
¶ Get the sensor tip location cartesian coordinates
Signature
GetSensorTipXyz()
Returns: the xyz values Return type: list of float New in version NX7.0.0.
License requirements: None.
SetSensorTipIjk¶
-
InspectionSensorBuilder.
SetSensorTipIjk
¶ Set the sensor tip location vector coordinates
Signature
SetSensorTipIjk(ijk)
Parameters: ijk (list of float) – the ijk values New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SetSensorTipXyz¶
-
InspectionSensorBuilder.
SetSensorTipXyz
¶ Set the sensor tip location cartesian coordinates
Signature
SetSensorTipXyz(xyz)
Parameters: xyz (list of float) – the xyz values New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Validate¶
-
InspectionSensorBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.