InspectionSaveToLayerBuilder Class¶
-
class
NXOpen.CAM.
InspectionSaveToLayerBuilder
¶ Bases:
NXOpen.Builder
Inspection Analyze Save to Layer dialog builder
To create a new instance of this class, use
NXOpen.CAM.InspectionOperationCollection.CreateInspectionSaveToLayerBuilderSel()
New in version NX9.0.1.
Properties¶
Property | Description |
---|---|
GroupName | Returns or sets the destination group name |
Layer | Returns or sets the destination layer |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetSelectedOps | Returns the selected operations. |
SaveToLayer | Saves measured data to a layer. |
SetSelectedOps | Sets the selected operations. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
GroupName¶
-
InspectionSaveToLayerBuilder.
GroupName
¶ Returns or sets the destination group name
-------------------------------------
Getter Method
Signature
GroupName
Returns: Return type: str New in version NX9.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
GroupName
Parameters: groupName (str) – New in version NX9.0.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Layer¶
-
InspectionSaveToLayerBuilder.
Layer
¶ Returns or sets the destination layer
-------------------------------------
Getter Method
Signature
Layer
Returns: Return type: int New in version NX9.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
Layer
Parameters: layer (int) – New in version NX9.0.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Method Detail¶
GetSelectedOps¶
-
InspectionSaveToLayerBuilder.
GetSelectedOps
¶ Returns the selected operations.
Signature
GetSelectedOps()
Returns: Selected operation tags Return type: list of NXOpen.CAM.CAMObject
New in version NX9.0.1.
License requirements: None.
SaveToLayer¶
-
InspectionSaveToLayerBuilder.
SaveToLayer
¶ Saves measured data to a layer.
Signature
SaveToLayer()
New in version NX9.0.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SetSelectedOps¶
-
InspectionSaveToLayerBuilder.
SetSelectedOps
¶ Sets the selected operations.
Signature
SetSelectedOps(selectedOps)
Parameters: selectedOps (list of NXOpen.CAM.CAMObject
) – Selected operation tagsNew in version NX9.0.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Validate¶
-
InspectionSaveToLayerBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.