InspectionPatternFeatureBuilderFeatureFilterTypes Enumeration¶
NXOpen.CAM.InspectionPatternFeatureBuilder.FeatureFilterTypes is an alias for NXOpen.CAM.InspectionPatternFeatureBuilderFeatureFilterTypes
-
class
NXOpen.CAM.
InspectionPatternFeatureBuilderFeatureFilterTypes
¶ Bases:
object
Filter for the list of available inspection features for inclusion in the pattern.
Enum Members
Enum Member Enum Member Description NotSet All inspection features will be listed Points Only point inspection features will be listed Lines Only line inspection features will be listed Planes Only plane inspection features will be listed Curves Only curve inspection features will be listed Holes Only inner circle, cylinder, and cone inspection features will be listed Pins Only outer circle, cylinder, and cone inspection features will be listed Spheres Only sphere inspection features will be listed Surfaces Only surface inspection features will be listed -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-