InspectionOutputOperationBuilderTypeOutput Enumeration

NXOpen.CAM.InspectionOutputOperationBuilder.TypeOutput is an alias for NXOpen.CAM.InspectionOutputOperationBuilderTypeOutput

class NXOpen.CAM.InspectionOutputOperationBuilderTypeOutput

Bases: object

Represents the output operation types

Enum Members

Enum Member Enum Member Description
Output1
Output2
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.