InspectionMeasDataBuilderBoundingType Enumeration

NXOpen.CAM.InspectionMeasDataBuilder.BoundingType is an alias for NXOpen.CAM.InspectionMeasDataBuilderBoundingType

class NXOpen.CAM.InspectionMeasDataBuilderBoundingType

Bases: object

Hole/Pin Matching Mode

Enum Members

Enum Member Enum Member Description
Bounded
Unbounded
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.