InspectionLinkPmiBuilderPointOrderTypes Enumeration¶
NXOpen.CAM.InspectionLinkPmiBuilder.PointOrderTypes is an alias for NXOpen.CAM.InspectionLinkPmiBuilderPointOrderTypes
-
class
NXOpen.CAM.
InspectionLinkPmiBuilderPointOrderTypes
¶ Bases:
object
Specifies the Point Order Optimization Type
Enum Members
Enum Member Enum Member Description Off No point order optimization will be done NearestNeighbor Point order optimization will use the nearest neighbor method ShortestPath Point order optimization will use the shortest path method -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-